NumericFunctions.Power function

Returns a number raised to the specified power

Format

ANSI-SQL Format:

POWER( Base, Exponent )

ODBC Format:

{{ FN POWER( Base, Exponent ) }}

Remarks

Returns Base raised to the power Exponent.

Base can be any Integer or Real numeric expression.

Exponent can be any Integer or Real numeric expression, (but must not be negative if Base is zero).

Example:

POWER( 2, 3 )

{FN POWER( 2, 3 )}


Disclaimer

ClearSCADA 2017 R3